Other Parts Discussed in Thread: TIDA-010015
I am looking at TIDA-010015 reference design which uses UCC28064A. In this design, two external gate drive ICs are used to drive the two MOSFETs in interleaved boost converters. Why are those external gate drives needed, compared to driving MOSFETs directly from GDA and GDB pins on the UCC28064A?
Looking at UCC28064A datasheet, GDA and GDB voltage is 12.4V typical (10.7 - 15V range). MOSFETs used are IPA60R120P7XKSA1. Their acceptable Vgs is +-20V, with Vgs threshold 3.5V typical (3-5V range). Should this mean that the MOSFETs can be driven directly from the GDA and GDB?