The customer is using BQ76942 test OCC (Over current charging function).
When OCC happen, the CHG FET will be closed, but the Discharge FET will keep turning on.
Then the charger is removed. The pack+ voltage will keep higher than BAT+.
Because the DSG pin voltage will leak to PACK+ via DISCHG FET GS 10M resistor.
So the Pack+ voltage will keep the high voltage state and it will not recover from OCC if there is no load in the pack+ and pack-.
Is there any good solution?