This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: the display light on the mainboard is always red and no function .

Part Number: TLV62569

1. The unit is used on automobile , so the issue must analyze and need a analysis report. Thank you.

2. The fail descripttion: the display light on the mainboard is always red due to the TLV62569DBVR (TI) PIN1 and PIN2  open circuit. The display light on the OK motherboard turns red for about 2 seconds than turning blue.

3. If the cause of the abnormal analysis is caused by EOS, please add de cap and verify the damaged area,and analyze the possible root cause .

4.