Other Parts Discussed in Thread: LP8866-Q1
Hi team,
Based on calculator tool of LP8866-Q1. if I use Dimming Frequency ≦4883Hz. "Might have audibale noise concern" this grid will show Yes.
So I searched the answer at datasheet. we can use phase shift mode to increases the load frequency, which can move potential capacitor noise above the audible band. Is there any other way to avoid audibale noise?
It would be better if there are other practical experiences that can avoid audibale noise.
BR,
Jimmy