Hi
My customer is developing a Camera module with PMIC (TPS68470) on Intel platform.
It’s hard to measure the total power current for these two IR-LEDs (flash mode) by power meter,
When we configured the value of “[10000]000” in the WLEDMAXF Register,
Does it mean that the max output current as 520mA in flash mode?
Could you help confirm that the actual current of WLED1 and WLED2 when the configuration?
Could you help check 520ma *2 is exceed the PMIC limitation (1000 mA)? Thanks.