This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV751: work condition confirm

Part Number: TLV751

Hi team,

I check that The TLV751 is a dual, adjustable, 500-mA low drop out (LDO) regulator. But I am not sure if 2 channel can provide 500mA at the same time, especially when their voltage between the input and output is large. Could you help check if the ambient temperature is 70℃, both of the output current is 500mA, and their voltage between the input and output is about 1~2V, can this device work normally?