Hello Team,
may I kindly ask you to provide the max current through the body diode in case reverse current is flowing while disabled, please?
Thank you and Best Regards, Hans
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hans,
We don't actually rate the body diode current as it's considered a parasitic path and the device isn't designed to have significant reverse current going through the FET. In the case of a reverse supply condition, the main FET actually turns on so that the power is dissipated over the main FET versus the body diode here.
Best Regards,
Tim
Hans,
Yes. The point here is that the exact current/power capability of the body diode is not characterized, however it is a lot less than the actual power FET itself. During a reverse supply condition we want the power to be dissipated over the main FET and not the body diode. Note that in order for automatic turn-on to occur, SEL1 cannot be floated or pulled high and must have some sort of path to ground (either pulled or through an MCU).
Best Regards,
Tim