I ask this question because there was no data in the datasheet for the conditions we use.
When using TPS7A2009PDBVR,
will the voltage supply be within the rated voltage range of the device to which it is connected (0.855 to 0.945V)
even if various factors (regulation, etc.) are considered
when the input voltage is 3.3V (25mV input variation after steady state) and load current is 250mA?
Best Regards
CIS Corporation
Quality Assurance Department
SAORI TSUKIJI