This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: CTRL pwm voltage

Part Number: TPS61169

Hi,

I would like to know If i power the vin of tps61169 with 3.3V, and the CTRL pin with a pwm signal voltage of 1.8V, it works or not works.

I read the datasheet and in page 10 is written: "The enable rising edge threshold voltage is 1.2 V", so i would to confirm if it is the case with a square pwm signal of 1.8 volts too. 

Thank's.