Hi,
I am currently trying to improve the charging feature of my PCB. Today my charge is set to 230mA as specified in the battery specifications (capacity of 1150mAh, standard charge current of 0.2C) but I need to accelerate it to 500mA (half of the max charge current which is 1C).
My schematic is the next one: .
Before changing the R137 I measured a charge current of 200mA which is compliant with the set limit (240mA), minus the current consumption of my Board (40mA). I changed R137 by a 430 Ohm resistor and the maximum charge current limit I reach in my tests is 385mA. This measure is not what I expected (385mA + 42mA is different from 500mA).
During my tests, I use a discharged battery at 3V. At the wireless charge beginning, I measure VRECT, IBAT and VBAT: VRECT = 5V, VBAT = 4.08V and IBAT = 385mA.
Do you think the BQ51050B difficulties to reach 500mA are due to the coil? Or the schematic?
In advance, thank you for your support. Best regards.