This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B-Q1: Design problem check

Part Number: BQ51013B-Q1

The functions of P5, P6, P15, and P16: P5 and P16 are overvoltage clamping pins, and the maximum voltage that the pins can withstand is 20V; P6 and P15 are communication modulation pins, which have the same electrical structure as P5/16 pins. 2. Capacitor function: filtering function, unable to prevent breakdown.

  • Hello

    P5 / P16 will control the clamp capacitors that will shift the resonant point and reduce system gain.

    P6 / P15 will control the communication capacitors to send data to transmitter for control of the system.

    Yes -- they have same voltage rating.

    Are you seen problems with your design?