This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2813-0: About frequency

Part Number: UCC2813-0

When determining the frequency using "UCC2813PWTR-0", there is a statement in the RC section of the delivery specifications to use the calculation formula below, but I do not know how much variation will occur from this calculation formula.

F=1.5/R・C

The Oscillator Frequency is stated as 46kHz±6kHz, but is it correct to assume that it will vary by this percentage (approximately ±13%)?

I would appreciate it if you could tell me about the variations in frequency.

  • Hi,

    There is no characterization at for this formula on the tolerance except at 46kHz. The tolerance in design is expected to be larger than 13% for the whole frequency range, you need to consider ±15% for UCC2813-0 when you design using this device.