Dears,
I am trying to make a new board based on the design of the evaluation board. I only added a Zener diode to regulate the output voltage from the ZA9710 transformer and changed the gate resistors to 10 ohms. However, when I try to use GUI to connect my board, it shows the hardware is connected, but I cannot move to the configuration 2 state, and all registers become zero. I try to load registers, but it still becomes zero. I checked the VCC1, VCC2, and VEE2, they are normal.
Could anyone give me a clue to do the further check?
Many thanks
Kexin