Part Number: TPS7H1111-SP
Other Parts Discussed in Thread: PSPICE-FOR-TI
Hi experts
Are there unencrypted PSpice models available for this device?
Thanks,
Jim B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS7H1111-SP
Other Parts Discussed in Thread: PSPICE-FOR-TI
Hi experts
Are there unencrypted PSpice models available for this device?
Thanks,
Jim B
Hi Jim,
The model for this device is unencrypted. The model for the main FET, which is used in this model, is required to be encrypted. Using this FET model allows for more accurate simulation and the ability to simulate things like PSRR. If there is a need, the encrypted FET model can be replaced with an unencrypted generic one for running general prototyping simulations. Alternatively, customers who don't have access to PSpice, can utilize PSpice-for-TI.
Portion of netlist where the FET is described is shown below. The model "nmos_1111" can be replaced/renamed with another FET model that the user adds a definition for in the netlist.
Drain Gate Source Bulk Model/Subcircuit Name
X_M1_U1 M1_N10438 G M1_N08730 M1_N08730 nmos_1111
Here is an example FET definition that shows the parameters that should be used:
.subckt nmos_1111_basic D G S B
MN1111 D G S B M1111
.MODEL M1111 NMOS
+ LEVEL = 5
+ W = 173094.56u
+ L = 1.41u
+ KP = 23u
+ VTO = 0.588155
.ENDS nmos_1111_basic
Thanks,
Sarah