This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25221: Continuous over current

Part Number: TPS25221


Hi

We are using TPS25221 in one our applications. The current limit resistor we use is 200K which corresponds to 275 mA current limit. I connected a 1A load along with an one ohm sense resistor and measured the voltage across the one ohm load. Please find attached waveform. Why is there a periodic dip in the current.