Hi team,
Customer has questions regarding to selection inductor & capacitor.
(The following references the equations in the data sheet.)
- Since the output is variable, there is no L that always satisfies equation (18).
There are higher or lower VIN-Vout. Which should they choose the L for? - What is the best inductor rating?
Is it OK if it is greater than 6.8A (high-side current limit) - For equation (23), is Δ Vout Voutmax-Voutmin?
What are the typical values to set?
Best regards,
Goto