I'm testing a prototype with related to this schematic using LMR33630ADDA:
Since in the layout the connection to AGND was missing I removed the IC and added a wire to ensure this connection ad soldered again the IC.
With Vin=12V, I get 2V inthe output instead of 5V.
IC sinks 120mA even with no load connected to the output and this is strange.
Assuming that everything was soldered properly, what could be the reason of this behaviour?
Thank you