This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3445: TRIAC dimmable wall light UK-US-EU

Part Number: LM3445

Good day,

I need to design a TRIAC dimmable device with 10 LEDs (3.2V @ 20mA). I was thinking of using the LM3445 since this seems to be a good option.

The requirements of the end product are:

  • compatible with UK-US-EU mains (90 - 260 VAC, 50 - 60 Hz)
  • compatible with most phase dimmers
  • safe
  • small - light will be fixed in wall socket

Is the LM3445 a good option or would it be better to search for an alternative?

Thank you for the support.