Other Parts Discussed in Thread: TPS50601A-SP
Hello,
I am using the TPS7H1101A-SP soft start, but when simulating with the PSpice model I am not getting the expected results. According to the soft start equation.
Using Css = 15nF would result in tss= 3.63ms.
However, after setting the enable to high the output voltage ramp does not start until after ~1.45ms delay.
Where is this delay coming from?
Below is the schematic and waveforms.