This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: BQ76920 cell voltage incorrect

Part Number: BQ76920

Hi

The customer design with BQ76920. The voltage of the first two cells is very small in one cell and very large in the other cell.  They used an oscilloscope to see that the collected voltage has stabilized.

But the AFE collect the voltage incorrect.

The schematic as below.

Please Help check the schematic.

Thanks

Star

  • Hello Star,

    I see that VC1 is connected directly to TS1. This is not good/okay, as there will be a constant current drawn through here and that will cause voltage inaccuracies.

    In our EVM we only use this for wake-up and it is only connected when pushing a button, we do not leave it connected.

    Best Regards,

    Luis Hernandez Salomon