This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075-Q1: Output Voltage Level

Part Number: BQ24075-Q1

Hi, 

I am using BQ24075-Q1 in my design. My VIN = 5V and my VBAT = 4.2V when battery is fully charged. 

From the datasheet it is confusing to find out what is the output voltage or the voltage on pins 10,11 connected to the load. Is it going to be 5V when VIN is available and 4.2V when VIN is not present? 

My configuration: EN1 = 0, EN2 = 1, SYSOFF = 0, CE = 0.

Please advise.