This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMS3655: current limit adjustable solution

Part Number: LMS3655

Hi,

My customer design requirement as below and they are looking for soft start and over current adjustable solution, could you please help to provide suitable solution?

1. input voltage 12~24V

2. output voltage 12V

3. Iout max 1.5A

4. OCP adjustable, if not, fixed 2.5A~3A is fine

5. soft start adjustable, if not, slew ramp up rate 4ms or greater is fine