Dear TI experts,
my customer considers TPS552872-Q1 for their new product.
But there are no WEBENCH simulation tool for TPS552872-Q1, so my customer have some problem to check the specification.
Is there any excel file or something else to check the specification?
and the condition of my customer is as below ;
Vin : 7V ~ 18V
Vout : 9V
Current limit : 1.5A ~ 2.0A 정도
Fsw : 500kHz
Please check this issue .Thanks.
Best regards,
Chase