Hello. I am Mr. Kang
I have a question while testing SMPS using LM5023MMX-2/NOPB.
I know you are busy, but I would really appreciate your reply.
The existing smps product operated in skip cycle mode at light load, so by changing the QR pin distribution resistor and capacitors R1, R2, Cd and CS pin resistor Rexternal, it escaped skip cycle mode and operated normally at the same load.
Iqr and cs offset voltages have increased. Will this have any effect?
Before change
Iqr: 0.5mA
VCS_OFFSET: 0.039V
QR pin voltage: 6.88V
After change
Iqr: 1.1mA
VCS_OFFSET: 0.12V
QR pin voltage: 6.66V
The datasheet recommends an Iqr value of 1~4mA. Will there be a problem if I deviate from this value?
Thank you.