Other Parts Discussed in Thread: USB2ANY, BQSTUDIO, , EV2400
Hi, we are facing a problem with the charging mode of the BQ25628 on a custom design (PMID is not used).
Although all the conditions are fulfilled (converter starts successfully, EN_CHG = 1, CE_N pin is low, no thermistor fault on TS, no safety timer fault), the device doesn't charge.
We have disabled the watchdog and have set all the voltage and current limits (reg0x02-re0x12).
We have read the charger status and fault status registers.
The CHG_STAT is 0x1 which indicates that the device is charging. However, the VINDPM_STAT is 0x01 (in VINDPM regulation) which is a bit suspicious as we expected 0x00 Normal mode.
No fault status recorded.
By reading the ADC conversions of the reg0x28-reg0x36, we see that the IBAT = 0 which means that the device isn't charging actually.
Could you please provide any further information why the charging mode is not working properly ?
We have also purchased the bq25628 EVM board with the USB2ANY interface. But it doesn't seem to work with bqstudio. Can you suggest a way to explore the EVM board with USB2ANY?
Thanks!