Hi,
We are looking at using TPS25200 to limit the input current in order to be compliant to IEC 62368 PS1 (I.e. below 15W) in a 5V device.
What happens in a single-fault condition for the Rilim and other necessary components?
Rilim open/not mounted I presume would limit the current to a low value, but what happens if Rilim is shorted to GND?
Would the current limit continue to increase or would it be clamped at ~2.9A? Would you then have to rely on thermal shutdown to turn off the device in case of a short circuit on the output?
Can you give an estimate of the time before this happens? (IEC 62368 PS1 requires the 15W limit to be enforced within 3 seconds)
Any additional information on the single-fault conditions would be appreciated.
Regards,
Jan