Other Parts Discussed in Thread: TVS2700, TVS2200, TVS1401, TPD1S514
Hi,
I need help to choose a TVS diode to protect a BQ24074. I'm not sure what clamping voltage is required.
I am making a small bluetooth household consumer electronics product (a baby motion sensor). It's powered by a 300mAh Lipo and charged at 100mA from USB VBUS.I'd like it to be capable of passing UL testing and I believe they test with VBUS set to 24v. Ideally I'd like the product to tolerate these voltages without damage and to fail safely otherwise.
The BQ24074 datasheet says the BQ24074 is tolerant of voltages up to 26V (28V max) and it has some inbuilt ESD protection.
Would the TVS2700 be a good choice? (https://www.ti.com/product/TVS2700)
Or the TVS2200? (https://www.ti.com/product/TVS2200)
any help is greatly appreciated.

My power section looks ilke this