Can we use the TPS7H2221-SEP when the input voltage is 5.45V?
The maximum voltage of TPS7H2221-SEP is 6V.
So If we apply the derating rule, we can use this switch until +5.4V.
- Linear voltage regulator = Vin * 90%
Should we consider the derating rule based on the ECSS standards?
- Linear voltage regulator = Vin * 90%