This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564257: Large output spikes.

Part Number: TPS564257
Other Parts Discussed in Thread: , TPS54620

Using the TPS564257EVM, I'm seeing large (150mV P-P) spikes with a 262mA load with a 1.05V output (As the EVM is configured, right out of the box). The data sheet shows less than 20mV P-P.

Measurements were made right at the EVM connector with a scope using one of those teeny ground leads Is this the expected behavior?. Please see attached scope captures.

Thanks,

Barry