Other Parts Discussed in Thread: TPS709, TPS7A20, TPS7A47, TPS7A24
Hi team,
TLV766-Q1 requires 2mΩ ESR as recommended operating condition.
While, the datasheet also states that "The device is designed to be stable using low equivalent series resistance (ESR) ceramic capacitors at the input and output". Some of ceramic capacitors have ESE which is less than 2mΩ depending on frequency.
Is requirement for minimum 2mΩ ESR correct?
I've never seen minimum ESR requirement for LDO which supports ceramic capacitor on output such as TPS7A20, TPS709, TPS7A24, TPS7A47 etc.
Best regards,
Shota Mago