This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS746: TPS74601

Part Number: TPS746

Hello, 

I am using TPS74601 to generate 3.3V o/p with i/p from 3.7V to 5V. I am not able to get expected o/p. Even I change values of F/B resistors R18  to 33K & R20 to 6.6K, Still o/p is not 3.3V constant. F/B pin voltage is stable 0.55V. Below are measured values at TP19. What can be wrong in this ?

 R20 &  R18 o/p Voltages (V)
Resistor Combination @3.7 ip @4.3 i/p @5 i/p
4.7k & 23.5K 1.9 +/- 0.2 2.5 +/- 0.2 3.2 +/- 0.2
1K & 5K 1.9 +/- 0.2 2.5 +/- 0.2 3.2 +/- 0.2
6.6k & 33K 1.9 +/- 0.2 2.5 +/- 0.2 3.2 +/- 0.2
55K & 275K 1.9 +/- 0.2 2.5 +/- 0.2 3.2 +/- 0.2