Hello,
I configured value of ALERT Pin Config register to 0x29. This means that ALERT pin is now configured as General Purpose Output,a REG1 regulator is used to drive output and that pin is driven active-high when controller to be drive high.
Everything works as expected - when command ACTIVE_HI (0x2812) is send, output goes to voltage of REG1 and when command ACTIVE_LO(0x2802) is send, output goes to 0 V.
The problem is at power-on - when BQ76942 gets a supply - output goes to high (there is a REG1 voltage on output) by default. Is it possible to config that output is on 0 V at power-on?
From which register is possible to read status of ALERT pin (to check if it is on high or low state)?
Many thanks,
Kind regards,
Dejan.