Other Parts Discussed in Thread: UCC28056, PFCLLCSREVM034
Hi,
I am designing a power supply with UCC256404 and a PFC pre-stage with UCC28056, based on a reference design PFCLLCSREVM034.
This is a 150W output power design, using an Itacoil LCC transformer, calculations are made with the UCC25640x Design Calculator Rev4.0.
Now I have trouble making this work properly, as soon as I put a load of more than ~90W, the UCC256404 stops working, no Rvcc is coming out and no switching occurs, the chip fails.
I notice that the Vcc under heay load rises to 25V or more (with no load it is 18V as expected with the transformer used).
I am a bit clueless as to what causes the chip failure, can you give me some hints ?
Of course I am willing to give more details about the design and the calculations if need be.
Kind regards,
Wim Verheyen for Joranalogue Audio Design.