Hi,
My customer design requirement is as below:
output voltage: 3.3V
output current: 3A
what's the min input voltage the device can support?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
TPS82130 has 100% duty cycle feature for lowest dropout, and the max duty/min input voltage is decided by below equation.
VIN(min) = VOUT(min) + IOUT*RDP.
RDP is typical 160mOhms so under 3A output, the min VIN is 3.3+3*0.16=3.78V.