Hi team,
Regarding the FB resistors (R1=1MΩ, R2=71.5kΩ at the datasheet), I understand that if the resistance ratio is not changed, there is no problem even if the resistance value is reduced by one digit,
However, as stated in the application note: https://www.ti.com/lit/an/slyt469/slyt469.pdf, we also understand that in general, if the resistance value is reduced by one order of magnitude, the phase compensation capacitance must be increased by one order of magnitude.
For the TLV61046A, is it unnecessary to add phase compensation capacitance even if the resistance is reduced by one digit?
For this application, I would like to insert a resistor in parallel with R2 and turn it on/off with a FET to make the output variable between 7~18V I would like to make the output variable between 7~18V by inserting a resistor in parallel to R2 and turning it on and off with a FET.
Example
At 7V output: R1=100kΩ, 12.7kΩ
At 12V output: R1=100kΩ, 7.15kΩ
At 18V output: R1=100kΩ, 4.64kΩ
Is it still unnecessary to add phase compensation capacitance for this type of usage?
Best regards,
Hayashi