I would like to know whether UCC2897A can support both bidirectional operation or not. As shown in the below figure i can be able to simulate it in forward direction. The input voltage 400v is stepping down to voltage around 14v if the load is a sink in the forward direction. Similarly i expect to step up the voltage in the reverse direction if the load is a source. Can you please provide some information on this.