I am facing UV problem for LP8764-Q1 on system reliability qualification. The fault report as following:
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5a r1
0x91
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5b r1
0x02
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5d r1
0x02
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x66 r1
0x01
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x69 r1
0x02
------------------------------------------------------------------------------------------
The log indicates the fault is caused by Buck3 interrupt with UV event.
mfg-s32g> i2ctransfer -f -y 1 w1@0x20 0x5d r1
0x02
Currently, I suspect this should be an OCP event causing Vout drop. Some of question should be clarified below.
- How is the definition of UV trigger level? Is this Vout*90%?
- OCP fault will be reported if the load current above the limit level for 30us, right? If we do not see this fault, the Vdrop might result from high transeint load or other reason?
BTW,here is current schematic. Please ignore the Iload information.