Hi team,
I have question about the 100% duty. If the input voltage is 5V and we want to ouput around 5V @ 1.5A, is there feasibility? I guess, it should be in the 100% duty mode and the output voltage should be 4.91V (Ron(60mohm)-Iout(1.5A)=Vdrop(0.09). Is it correct? we cannot see the minimum off time at 5V. could you tell us it? In addition to this, what the required input voltage not to in the 100% duty mode?
Best Regards,
Uchihara