This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: LM5118

Part Number: LM5118


Hi,

  1. Vin(min) - 9V
  2. Vin(max) - 69V
  3. Vout - 12V
  4. Iout - 3A

For the Enable signal, we are planning to use a GPIO from controller to toggle the pin. In datasheet it has been mentioned that, Enable pin status as per the voltage across the pin

<0.7V - Enable is LOW , IC is off

>3V  - Enable is High - IC in Normal operation.

So, can we directly connect a GPIO of 3.3V on EN pin to control the IC. Or do we still need to use BJT or MOSFET to have a level shifting?

Regards,

Hareesh