Hello,
I designed a circuit for lithium ion battery charging with the BQ24040. I tried to figure out why the battery does not charge but after some days of studying the data sheet and measuring the outputs I don't know how to solve this problem. I tested the circuit with an USB-Adapter power source, with and without the battery connected to the output but there were no changes. I tried the circuit with TS-PIN floating but there were no changes at all.
The circuit is shown below and my measured values from the ic-pins are the following:
IN = 5,2V (from USB Power source)
OUT = 3,53V (the actual cell voltage but without any kind of charging)
CHG = 2,7V
PG = 0,0V
ISET2 = 5,2V
ISET = 0,0V
PRE-TERM = 0,0V
The data sheet contains just the info that:
CHG (HIGH) = no charging
PG (LOW) = input voltage above Uvlow and Vout
I would appreciate any help or tips you can give. Thank you!