This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: Power management forum

Part Number: LM5148
Other Parts Discussed in Thread: LM25149-Q1EVM-2100, LM5149-Q1, LM5149-Q1EVM-400


Hello,

I am currently in the process of constructing a buck converter with the following specifications:

Input Voltage: 15-80V

Output Voltage: 12.51V

Output Current: 10A (Maximum)

  • During testing, I encountered the following issues:

            1.The integrated circuit (IC) is getting damaged under both load and no-load conditions.
            2.When I increase the voltage, the IC heats up and eventually gets damaged.


I have attached my schematic for your reference. 

I am seeking suggestions for improvement and kindly request your support in resolving this issue. 

RM-004-V-00.SchDoc