Other Parts Discussed in Thread: BQ27426
We are trying to generate a ChemID for an LFP battery and have tried multiple times and have been getting wildly incorrect results, with results that give Lithium cobalt matches. Can best practices be shared for chemid identification? I have also noted in manuals that one can send cells to TI for chem ID generation and matching.
Typical output is given as below:
Chemistry ID selection tool, rev=2.54
Configuration used in present fit:
ProcessingType = 2
NumCellSeries = 8
VoltageColumn = 2
CurrentColumn = 3
TemperatureColumn = 4
ElapsedTimeColumn = 1
Best chemical ID : 414 Best chemical ID max. deviation, % : 18.54
Summary of all IDs with max. DOD deviation below 15%
Chem ID max DOD error, % Max R deviation, ratio
0 0 0
Warning: Deviation is above recommended level. New chem ID needs to be released for this cell. Please contact your TI representative to send the cell to Dallas for characterization
Selection of best generic ID for ROM based devices like bq274xx
Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27411-G1C: 4.35V LiCoO2 26.93
3142 bq27421-G1D: 4.4V LiCoO2 29.24
128 bq27421-G1A: 4.2V LiCoO2 40.08
312 bq27421-G1B: 4.3V LiCoO2 97.39
Best generic ID 354
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
Device / Family #2
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 26.93
1202 bq27621: (default) 4.2V LiCoO2 28.8
1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 30.42
Best generic ID 354
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
Device / Family #3
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3230 bq27426: (default) 4.35V LiCoO2 24.11
1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 28.8
3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 29.24
Best generic ID 3230
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule