Hello,
I am designing a converter with LM5118. In this process, I follow the typical application in the datasheet. However, I noticed some errors in the calculations and I would like to both report and confirm them.
The first error is the Iripple (buck) calculation on page 27. It is calculated as 3.36 in the datasheet, but I calculate the result as 2.86. The second is the k (buck) calculation on page 28, calculated as 1.16 in the datasheet, but I calculated it as 1.33.
In addition, how big can we choose the k value to keep R(sense) at the desired value, can there be a problem of exceeding the upper limit?
Thank you very much in advance.