Other Parts Discussed in Thread: TPS62816-Q1, TPS62870, TPS54618
Hi TI,
Could TPS62867 disable tDelay and fast tRamp?
I'd like to turn on the power faster when EN is high.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
Could TPS62867 disable tDelay and fast tRamp?
I'd like to turn on the power faster when EN is high.
Hi,
No, this is not possible. What is your startup time requirement? Do you need to support a 6A load?
Other 6A devices that startup faster are TPS62816-Q1 and TPS62870.
Chris
The requirement is 0.5ms could finish ramp-up after EN is asserted.
Is there any suggestion about TI's solution?
I'll check start-up timing of these two parts.
Thank you for sharing your SS time need.
TPS62816-Q1 and TPS54618 have faster startup. Would either of these work for your application?
Chris