Other Parts Discussed in Thread: TPS65994
Please tell me about PDC TPS65994.
A. About Config INPUT
# Used for sink device.
#data lane is used in the following case
- USB2.0
- DP Alt-mode(4Lane)
- USB2.0 + DP Alt-mode(4Lane)
# VBUS input voltage should be up to 15V.
# EEPROM is to be implemented for F/W.
In the above case, is "SafeMode" OK for the mode specified in ADCIN1/2 (Config INPUT)?
B. About GPIO4/5,
The datasheet says to connect "USB_HS" when supporting BC1.2.
Although it is necessary to receive power, it is not necessary to comply with the BC1.2 standard.
In this case, I can just connect it to GND, right?
Best regards,
Hirakawa