This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS784-Q1

Hello Support Team
On the TPS78433QWDRBRQ1 the EN is pin7 (pin6 is not connected) and on the B-Version TPS78433QBWDRBRQ1 the EN is pin6 (pin7 is not connected). The data sheet states that the respective unconnected pin should be connected to GND or floating. Can I create a single layout (pin6 and pin7) on IN, or should I better create two footprints?

Many thanks in advance
Beni