This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: Inductor Substitution

Part Number: TPS61169

The TPS61169 datasheet includes recommended inductors, which makes me think that there might be reasons for similar inductors to not be suitable? Specifically, the recommended inductors are not easily available to me so I'm wondering if there's any reason not to use a TDK VLS6045EX-100M?

- 10 µH, ±20%

- 3.4 A

- 3.9A saturation

- 47 mOhm 

Thanks in advance!