Other Parts Discussed in Thread: TPS61060, TPS61158, , TPS92360, TPS61166, TPS61165
Hello,
See attached picture for a summary of what I am looking for. LED driver application (5x LEDs in parallel). I am looking to separate the LED driver bias and LX supply rails, to accommodate a supply rail (VSUP as drawn) that can droop considerably below the input voltage range of TI's LED drivers.
Here is the info in text form:
Vin (labeled VSUP in picture): 0.5V to 3.2V. The 0.5V would be absolute worst case.
Vbias: 3.3V
LED Vf: 6.4V maximum
LED forward current: 100mA maximum total @ 100% duty cycle
Method of dimming will be PWM, ideally >20kHz to avoid any audible cap issues.
Is the drawing attached possible with TI's DC/DC solutions? I can't seem to find a boost or LED driver solution that can handle such a low input voltage, while also supporting an output voltage > 6V using the standard supply rail topology. I am hoping to avoid chaining 2x DC/DC converters together due to the inefficiency hit.