This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988: PD pass through dock station

Part Number: TPS65988

Hello there,

I'm looking to create a dock station using TPS65988 without using an external DC adapter. I want to connect a PD charger to Port B and charge the device connected to Port A via PD. Is it possible to achieve this without using an EC, relying solely on configuration?

Thanks,

Sam

  • Hi Sam,

    Unfortunately, no, the TPS65988 does not support true PD passthrough without the addition of an external EC. The advertised Source capabilities for port A do not currently have a way to take into account the active PDO contract on Port B and modify the power levels accordingly.

    Thanks and Regards,

    Chris Lim