Other Parts Discussed in Thread: LM76005
Hello,
The same question came up in the forum but w/o clarification within this forum. I do not understand the mismatch between the EC data and the description in the text:
- VENH in the text should be VEN_VOUT_H from EC data (typical value) = 1.204 V
- VENL in the text should be VEN_VOUT_H - VEN_VOUT_HYS (typical value) =( 1.204 - 0.15) V
Howevr, in the text VENH = 1.218V and VENL = 0.99V is used. What is the background of those values? I know for worst case analysis I have to consider the extreme values for VEN_VOUT_H. For hysteresis only a typical value specification exists.
Furthermore the values in the application section (above) are not in line with the section 7.3.4 in datasheet:
For this I would use the EC data. How to cope with the different values?
Thanks and best regards
Andreas N.